What Accessories are included inside the box/packaging of Smart-UPS Ultra 8kW and 10kW 230V models (SRTL8KRM4UI and SRTL10KRM4UI)?
There are questions regarding the accessories that are included in the packaging
Answer:
SRTL8KRM4UI / SRTL10KRM4UI-APC Smart-UPS Ultra Online Li-ion 10kVA 230V expected accessories:
| Part Name | Manufacturing Part Number | Description | Qty |
| 1.Battery | SRYLBM | Internal battery | 2 |
| 2.Bezel | 0M-102830A | Front Bezel | 1 |
| 3.Railing kit | 0M-756H | Rack mounting kit | 1 |
| 4.Litkit assy. | 0L9787B | mounting accessories | 1 |
| 5.Sensor | AP9335T | Temperature sensor | 1 |
See actual images
1. 2pcs of Battery Modules ( SRYLBM)- can be found at the top upon opening of the box/packaging. (see image below "Figure A")
FIGURE A:
2. Bezel - can be found underneath the battery packaging (see image below at "Figure B")
3. Railing kit - can be found underneath the battery packaging (see image below at "Figure B")
IMAGE B:
4 Lit-kit assembly - can be found at the side of the box (near the UPS)
see content below at "Figure C":
FIGURE C:
5. Temperature Sensor (AP9335T) - can be found near the lit-kit assembly (see "Figure D")
FIGURE D: