Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
EcoStruxure Operator Terminal Expert - Backup and Restore recipe remotely.

Issue:

Is there any tool to backup and restore recipe file from HMI Target remotely (like Vijeo Data Manager does in Vijeo Designer) ?

Product Line:

EcoStruxure Operator Terminal Expert v3.5 SP1 and all previous versions.

Resolution:

No, there isn't any tool like data manager in Vijeo Designer.

For reference, FTP is not supported from the cyber security point of view, and R&D already had the plan to support FTPs in future version, then it should be able to backup and restore recipe file remotely. This feature has been implemented starting with version 4.0 of Operator Terminal Expert.

With previous versions, user can export related recipe file to USB memory stick.

In the Recipes - Control, set the Export/Import Data Location to USB Storage and define the folder Name.

Recipe Control setup for export/import to USB.

On the recipe screen, program some switches to execute the scripts to Export and import the recipes.

Recipe export/import scripts.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)