Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What conditions are needed to set %S51?

The initial value of %S51 is 1 (after a factory reset), meaning that the RTC has not been set. After the first successful write to the real-time clock (RTC) with valid data, %S51 will be set to 0.


One of the following conditions must be true in order for %S51 to be set to 1:

  • Hardware RTC is not present
  • Hardware RTC is not readable or writeable
  • Hardware RTC has never been updated
  • Hardware RTC contains an invalid date/time (ex. 31 February)
  • Hardware RTC does not update correctly from second to second or is just frozen
Note: The data written to the RTC does not have to be the current time.