Hôm nay chúng tôi có thể giúp gì cho bạn?

Is there a "T" fitting for the Power busbar PBCE5A225ST120B?

Issue:

Needs a "T" fitting for Powerbus busway

Product Line:

Busway

Environment:

PBCE5A225

Cause:

N/A

Resolution:

For Powerbus applications that require a tee, a cross should be used and the unused end should be

capped off