Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How to communicate between two M580 PLC using OPCUA client on M580 firmware 4.xx ?

Article available in these languages: Tiếng Nhật

The video will show the step to follow in order to connect to the M580 CPU to an external OPCUA Server by using the Function Block of OPCUA client embeded in the M580 firmware 4.xx.
You will find as well the tutorial application used inside the video in order to give you an overview on how to program it.
In the tutorial application, you will find the "ReadList Method" used inside the video and you will find an example on the "UA monitoring method by subscription".
1_Tutorial M580 OPCUA client application.sta : this is the OPCUA client application
2_Tutorial OPCUA Server application.sta : this is the OPCUA Server application by using BMENUA0100 module (with version 2.01)


Schneider Electric Việt Nam

Phần đính kèm
Tutorial M580 OPCUA client application.zip [119.64 KB]