Hôm nay chúng tôi có thể giúp gì cho bạn?

What firmware version of the BMECRA31210 is required for the when using the Profibus module PMEPXM0100 in a remote drop?

Issue:
Minimum firmware version of the BMECRA31210 required when using the Profibus module PMEPXM0100 in a remote drop


Product Line:
PMEPXM0100, EcoStruxure Control Expert


Resolution:
BMECRA31210 version V2.40 is required if the Profibus module is used in a remote drop.