Hôm nay chúng tôi có thể giúp gì cho bạn?

NetBotz camera pod NBPD0165 occasionally changes to black & white image in well lit room.

Issue:
NetBotz camera pod NBPD0165 occasionally changes to black & white image when in a well lit room.

Product Line:
NetBotz

Environment:
NBPD0165 camera pod

Cause:
The NetBotz 165 camera pod has both day and night capabilities. When in night mode / dark mode, the image changes to black and white.
There are occasions where the image will change to black & white during the day or when in a well lit room.

Resolution:
Please log on to the camera directly.

Find the setting under "IR Function" for "Day/Night Threshold".

Change night to day setting from 7 to 4 as per the following image.

Camera Menu