Can Auxiliary Contact Blocks Be Mounted When Using GV2GH7 Line Spacer?
Using the GVAE auxiliary contact blocks when GV2GH7 line spacer is used on GV2P Motor Circuit Breakers
Product Line:
GV2P, GV2
Environment:
Contactors and Starters
Resolution:
Front mounted auxiliary contact blocks (GVAE**) when a GV2GH7 line spacer cannot be mounted. Recommended to use the Left Hand Side Mounted auxiliary contact blocks (GVAN**) instead.