APDU10K web interface only shows Celsius
Issue:
The web interface of an APDU10K series PDU only shows temperature readings in Celsius, while the front display supports both Fahrenheit and Celsius.
Product:
Netshelter RackPDU Advanced models, part numbers starting with APDU10
Environment:
PDU's with an optional temperature probe connected, APDU1335T/APDU1335TH
Solution:
The APDU10K series support Fahrenheit and Celsius temperature scales on the front PDU display, but the web interface supports only Celsius. Support for both temperature scales will be added in a future firmware release, and this article will be updated when that version is available.
Đã phát hành cho: Schneider Electric Việt Nam