How to run Process Drives with a small or no motor
Issue:
How to run Process Drives with a small or no motor
Product Line:
ATV630/ ATV930
Environment:
Open Circuit
Cause:
n/a
Resolution:
Go to Complete Settings, Then select Motor Parameters, scroll down to Motor Control Type- set to U/F VC 5 pts then go to Error/Warning Handling- Output Phase Loss- set to Function Inactive.