Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
NetBotz graphs plot only 2 data points
Issue:
NetBotz graphs have only 2 data points

Product Line:
NetBotz

Environment:
NBWL0755
NBRK0750

Cause:
NetBotz sensors that do not change will only show 2 data points in a graph. For instance, a door sensor that has not opened will have a closed State at the beginning of the graph and at the end. No other points will be recorded. The same will be seen for a temperature sensor if the temperature has not changed.

Conversely, if there have been multiple changes, you should see multiple points on the graph.

Resolution:
Upon checking Sensor data history excel, it shows all sensor data captured during this time period.

This function works as designed.