Issue:
After upgrade to (Nutanix Cluster Check) NCC 4.6.2 the AHV root account gets locked out if the password is changed. This will prevent PowerChute from shutting down AHV hosts.
Product:
PowerChute Network Shutdown
Environment:
Nutanix AHV host, NCC 4.6.2
Cause:
The AHV root account gets locked.
Solution:
Upgrade NCC to version 4.6.3. Please refer to the following Nutanix Knowledge Base article - https://portal.nutanix.com/page/documents/kbs/details?targetId=kA07V000000H4dZSAS
Đã phát hành cho: Schneider Electric Việt Nam