Hôm nay chúng tôi có thể giúp gì cho bạn?

Can we using ZB4BZ021 on XD4PA14 to achieve flush mounting?

Even if it is possible to assemble XD4PA14 joystick in the ZB4BZ021 flush kit.
It will not perfectly fit : The joystick will be 1 mm above the flush accessory. So it depends on customer's sense of aesthetic !