Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Can IO Scanner be modified in an M580 Hot Standby system without interruption?

Issue

Looking to add, remove or modify devices from the NOC or CPU DTM. Can this be done without process interruption?

Resolution

Yes, this can be done. As of Unity V12, all Control Expert and v2.8 of M580, the ability to apply an offline application modification and return to a Standby state was introduced.  This is accomplished using the HSBY_BUILD_OFFLINE block. It supports modifications that require an offline BUILD CHANGE. It will not support ReBuild All modifications, only Build Change.

Attached is a document which outlines this feature.

Schneider Electric Việt Nam

Phần đính kèm
M580 HSBY Adding a Device while Process Running v2.0.pptx.zip [997.18 KB]