Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How do you run a small test motor with the ATS480 soft start?

Issue:
How do you run a small test motor with a ATS480 soft start?

Product Line:
ATS480

Environment:
Small test motor

Cause:
n/a

Resolution:
Go to Menu 3.3: Set [Small Motor Test] SST to YES. The PHP (Phase Loss Monit) will be forced to NO and Control Mode (CLP) is forced to Voltage Control (VC).
To start the test, apply a Run command to the soft starter by pressing the RUN button on the display terminal or via the STOP and RUN control terminals.
To stop the test, apply a Stop command to the soft starter by pressing the STOP / RESET button on the display terminal or via the STOP and RUN control terminals.

Note:
The [Small Motor Test] SST test function is set to [No] when the soft starter control supply is disconnected.
Upon next power-up the soft starter, including [Phase Loss Monit] PHP and [Control Mode] CLP, will return to its previous configuration.