Hôm nay chúng tôi có thể giúp gì cho bạn?

Does ATS01 have a Fault Reset?

The ATS01 soft starter does not include a fault reset function and is not capable of generating or displaying fault codes. For this reason, it requires an external overload relay (OLR) and contactor to interrupt the circuit in the event of an overload condition.