Issue:
Disable the cyber security password feature on the ATV340 Drives.
Product Line:
ATV340E version
Environment:
Ethernet version only
Cause:
Disable feature.
Resolution:
If your ATV340E drive has firmware version V3.2IE26 or above, it will have a cyber security feature that will require you to enter a password when you connect over Ethernet. If the law does not permit, you to have a cyber security network you can disable the feature after you have changed the original password.
If you opt to disable the cyber security feature, you do so at your own risk.
Đã phát hành cho: Schneider Electric Việt Nam