Hôm nay chúng tôi có thể giúp gì cho bạn?

What can cause a Somove "Error while executing service 'CheckPhysicalReference' with arguments"?

Issue:

Somove "Error while executing service 'CheckPhysicalReference' with arguments.

Product Line:

Somove and ATV630 Drive

Environment:

All

Cause:

Somove will not connect to the ATV630 or ATV930 series Drive because of an inop Main control board.

Resolution:

You will see this error in somove if you are not able to connect to the Drive using the TCSM cable or Ethernet in this case there appears to be an issue with the Drives main control board, and it will need to be replaced.

Note

The MCB or Main Control Board part number for the ATV630 or ATV660 drive is VX4B600100 and the ATV930 drive is VX4B900100.

Note: In the US and Canada this part is intended to be installed by Schneider Electric Field Services or their delegates, since it may require special software to be used to ensure its compatibility with the VFD.

If this is done by someone else, there is no guaranty it will work.

somove error