Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Do I need to fill the lubrication reservoirs of the Lexium™ MC12 carrier (LXMMC12CA51S100) before using it for the first time?
The lubrication reservoirs of the Lexium™ MC12 carrier (LXMMC12CA51S100) must be filled before first use.
This can be done with the carrier mounted on the rail or removed from the rail.
If the lubrication nipples are covered by a tool mounted on the carrier, you must disassemble the tool.
Details of lubricants are given in the Lexium MC12 Multi Carrier Hardware Guide.
NOTE: Exposed or uninstalled carriers must have the protective cover of the drive magnets installed at all times. The cover is only removed at the time of carrier installation.