Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
E3SOPT001 SSH CBC Detected
Issue: Detection of CBC (Cipher Block Chaining) ciphers being enabled in SSH, which can be flagged by vulnerability scanners

Environment:
E3SOPT001 Firmware 3.7.DA807.APC.19 and lower

Cause:
Vulnerability scanners detect CBC ciphers as a potential security vulnerability in SSH configurations, which is the cause of this issue.

Solution:
The SSH ciphers will be updated on future firmware release.  Please note that an exact ETA for the update is not available at this time. This FAQ will be updated accordingly.

Note: SSH uses the highest preference cipher that both the server and client support, which means it will prioritize the most secure cipher available.

If you have further questions or need additional information, please reach out to your local Customer Care Center. Check the link below and set the correct country.
How to Contact APC - APC USA

Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Tìm hiểu thêm
Sản phẩm: