Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What is the correct part number of the SYMMETRA LX Tower Frame Caster (Front and Rear)?
Issue: What is the correct part number of the SYMMETRA LX Tower Frame Caster (Front and Rear)?

Product Line:
ALL SYMMETRA LX TOWER TYPE FRAME  (Power and XBP)

Environment:
All Serial Numbers

Cause:
In unexpected circumstances there are events where sometimes there are modifications or moving of such set-ups to another location which results in a lot of movement of the frame and possibly damage to the caster. And to know the correct part number of the particular caster it is good to know each position and its corresponding part number and description.
Answer:

Symmetra LX does have 4 pcs. of caster:

See the following images below for full details:

Caster 1.JPG

Complete image description of the following casters. (see below)
correct description.JPG
See provided link below for your references:

SYAFSU7 = https://www.apc.com/us/en/product/SYAFSU7/apc-symmetra-lx-castor-kit-    right-front-left-rear/

SYAFSU6 = https://www.apc.com/us/en/product/SYAFSU6/apc-symmetra-lx-castor-kit-left-front-right-rear

Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Tìm hiểu thêm
Sản phẩm: