Hôm nay chúng tôi có thể giúp gì cho bạn?

How to Brain Dead an Easy-UPS (Full UPS Logic Reset)

Issue:


To brain dead an Easy-UPS is to purge the charge in the brain of the UPS.


Product Line:


Easy-UPS Line-Interactive, Easy-UPS Online


Environment:


All serial numbers.


Cause:


Troubleshooting procedure often prescribed to clear some faults or unwanted behaviors.


Resolution:


To do this, follow the below procedure;

1: Disconnect any attached load.

2: Unplug the UPS from the wall socket.

3: Disconnect the UPS' internal battery or the battery disconnect switch if any.

4: Push and hold the ""On"" button on the UPS for 5 seconds

5: Reconnect internal battery or battery disconnect switch if any.

6: Plug UPS in to known good power source.

7: Turn UPS on.