Why can't SSOLR be used with M10 factory form (Marine certification) in Motor Starters?
Solid state overload relays are not available for marine certification
Product Line:
9065SF Overload Relays - GIC Product
Environment:
US Product
Cause:
Certification
Resolution:
For the SSOLR there are two reasons that left this component off of the testing and certification process:
1) part of the marine requirement is that ALL current carrying parts are COPPER. The control circuit component of the MotorLogic that is supplied with the product is not and therefore would not meet the criteria.
2) Since it would require a redesign of the above component it has since never been updated to include the SSOLR.
Đã phát hành cho: Schneider Electric Việt Nam