Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How to avoid gcc compilation error after upgrade from BMEP584040 to BMEP585040
In CE15.3, a GCC compilation error may occur after changing the CPU in the application from BMEP584040 to BMEP585040 or higher. This issue arises when a few not recommended instructions are used in specific sections.
The compiler utilized in BMEP585040 and higher models differs from the one used for BMEP584040 references and lower. This imposes limitations in ST sections, particularly when 'JMP' instructions are used in an infinite loop (e.g., with labels).
To prevent potential GCC issues, it is strongly advised to replace these 'JMP' instructions in infinite loops with 'While' instructions.

See the following example:

The following code uses label and JMP instructions:

Code uses label and JMP instructions

Can be replaced by this one, doing the same thing, and able to be built by the BMEP585040 compiler:

Code uses while instead