Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
PowerChute Serial Shutdown does not report a self-test has run when connected to a Back-UPS.

Issue:
PowerChute Serial Shutdown does not report when a self-test has been run when connected to a Back-UPS if a user presses and holds the Back-UPS's power on button to trigger a self-test. Also, a Back-UPS will run a self-test every 14 days from the date/time of the last self-test. When the UPS triggers the scheduled self-test, PowerChute will not record that the test has been run.

NOTE: If you initiate a UPS self-test via the PowerChute UI diagnostics page for Back-UPS models, the result may return as “Unknown.” If this occurs, then try initiating the self-test again. If the issue persists, your Back-UPS may not support manual self-tests. See Schneider Electric FAQ000266376 Self-test fails on Back-UPS when the test is run from PowerChute Serial Shutdown

Products:
PowerChute Serial Shutdown
Back-UPS

Environment:
PowerChute Serial Shutdown connected to a Back-UPS.

Cause:
A mistranslation of the event by PowerChute.

Solution:
This issue will be resolved in a future release.