Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Single Phase Symmetra UPS Frame Life Expectancy

Question:
An old APC UPS has a valid failed battery issue. Would it be a better time to consider a new unit over a new battery?

Product:
Single Phase Symmetra units


Answer:

The frame of the Symmetra unit is the main housing of all the removable modules (e.g. Power Module, Battery Module, Intelligence Module) of the whole unit build. This is the critical point of failure which is the main reason why this component is made to be robust. However, all products may it be from any brand would have its own life expectancy.

As related to public kbase FAQ000265093, the Symmetra frame is also expected to last 7 to 10 years. It is highly advised that we take advantage of the Trade UPS program if a if a Symmetra Frame is at 10 years or older.

A document is also found in knowledge base FAQ000239442 would also outline the recommended life cycle of a Symmetra UPS.

We recommend to please contact our Technical Support Agents at 1-800-800-4272 or chat with us at APC by Schneider Electric to properly troubleshoot your UPS prior to any replacement.