Hôm nay chúng tôi có thể giúp gì cho bạn?

How can the Advantys STBNIC2212 V3 be replaced with a V4 module in a CE application?

  • Open the DTM in the CE application.
  • Click on Start Advantys to start tthe Advantys Configuration software and link it with the DTM..

ewtyutr

  • Right click on the STBNIC2212.
  • Select 'Replace NIM'.

rettrwe

  • Replace the STBNIC2212 V3 with the V4 module.

fgggg

  • Save the changes.
  • Build the Advantys application.
  • Save the changes.
  • Set the rotary switches on the V4 module to the same position that was on the V3 module.
  • Power cycle theSTBNIC2212.
  • If the rotary switch is set to the 'Stored' position: (See below)
    • Open the web page for the STBNIC2212.
    • Assign the same IP address and
    • Leave the Device name blank in the web pages for the to the new STBNIC2212 .

ewewre

  • Power Cycle the STBNICC2212.
  • Ensure that the Advantys island is in a ready state..
  • Go back to CE.
  • Apply the changes to the DTM.
  • Rebuild.
  • Save the changes.

ewqfrf

  • Connect to the M580 PLC.
  • Transfer the CE application to the PLC.
  • Connect to the STBNIC2212.

ewqfff