Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How do I Upgrade the Firmware on my Schneider Electric Advanced Rack Power Distribution Unit (APDU10K) unit via USB?

Question:

How do I Upgrade the Firmware on my Schneider Electric Advanced Rack Power Distribution Unit (APDU10K) unit via USB?

Product Line:

  • Standalone Schneider Electric Rack Power Distribution Unit (APDU10K) ONLY
  • APDU10250SM, APDU10250ME, APDU10151SW, APDU10151SM, APDU10151ME, APDU10150SW, APDU10150ME, APDU10150SM


Cause

Users may wish to upgrade their firmware to take advantage of enhancements, bug fixes, or new features. Also, sometimes a firmware upgrade can be interrupted or unsuccessful and these instructions can be followed to remedy the problem.

Typically, these upgrades do not require the device the Network Management Card is installed in to be powered down or cause unnecessary downtime.

Resolution

Download Firmware

Update Firmware

1. Go to www.apc.com and download the most recent firmware version, apc.fw

2. Extract the apc.fw and copy its contents to the USB.

Note: USB drive doesnt need to be formatted to FAT32 file system. Copy the firmware file only to the USB Flash Drive.

File Content

3. Insert the USB drive into the USB port on the Rack PDU.

Insert USB

4. Go to Settings>USB on the LCD display of the Rack PDU.

Settings Option

USB Option

Note: If USB is not detected, this message will appear.

No USB Detected

5. Select Firmware Upload from the menu and select Yes to confirm.

NOTE: The LCD display will show the Firmware update progress. When the update is complete, the Rack PDU will automatically reboot.

Firmware upload option

Firmware Upload

6. Remove the USB drive from the Rack PDU.

7. Go to Settings>Device>Firmware to confirm that the firmware uploaded successfully.

If you have any clarifications and/or requests for the above mentioned available information, please feel free to contact us at 1-800-800-4272 or chat with our technical support representatives.

Schneider Electric Việt Nam

Phần đính kèm
2.0.8.2 2.zip [40.15 MB]
Tìm hiểu thêm
Sản phẩm:
Tìm hiểu thêm
Sản phẩm: