Hôm nay chúng tôi có thể giúp gì cho bạn?

IDP10-T/IGP10-T Calibrate at Known Tank Level

X = Actual value to be displayed

Y = Original M1 LRV value

  1. Press the NEXT button and the word RERANGE will be displayed.
  2. Press ENTER and M1URV will be displayed
  3. Press NEXT and M1LRV will be displayed
  4. Make note of this value as the “Y” value
  5. Press ENTER and left hand most digit will blink. Press NEXT until this digit is equal to the most significant digit of the “X” value
  6. Press ENTER and the next digit will flash
  7. Press NEXT until this digit matches the value of the next most significant digit of the X value. Repeat procedure for the remaining digits until the entire X value has been entered
  8. Press ENTER and Place DP will be displayed
  9. Press NEXT until the decimal point is in the correct location
  10. Press ENTER and CANCEL will be displayed
  11. Press NEXT and SAVE will be displayed
  12. Press ENTER and device will be returned to Measurement Display
  13. Press the NEXT button 3 times and CALIB will be displayed
  14. Press ENTER and display will indicate CAL AT0
  15. Press next and display will indicate CAL LRV
  16. Press the ENTER button and display will indicate CAL WAIT and then display LRVdone
  17. Press NEXT 6 times and SAVE will be displayed
  18. Press Enter
  19. Press the NEXT button and the word RERANGE will be displayed.
  20. Press ENTER and M1URV will be displayed
  21. Press NEXT and M1LRV will be displayed
  22. Press ENTER and left hand most digit will blink. Press NEXT until this digit is equal to the most significant digit of the “Y” value
  23. Press ENTER and the next digit will flash
  24. Press NEXT until this digit matches the value of the next most significant digit of the Y value. Repeat procedure for the remaining digits until the entire Y value has been entered
  25. Press ENTER and Place DP will be displayed
  26. Press NEXT until the decimal point is in the correct location
  27. Press ENTER and CANCEL will be displayed
  28. Press NEXT twiceand SAVE will be displayed
  29. Press ENTER and device will be returned to Measurement Display
  30. Complete