Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
My SRTL3KRM1UNC, SRTL3KRM1UC, SRTL2K2RM1UNC and SRTL2K2RM1UC will not upgrade the UPS FW over the NMC Web interface

Issue:
There is likely an issue will be encountered while trying to upgrade the UPS FW over the web interface


Product Line:
SRTL3KRM1UNC, SRTL3KRM1UC, SRTL2K2RM1UNC and SRTL2K2RM1UC

Environment:

All part numbers, all serial numbers

Resolution:

It is recommended to use SCP or SSH if upgrading the UPS firmware remotely.  Please see the following steps for the procedure.

Steps

  1. Use “scp” to transfer firmware image file to root folder of NMC. For example: “scp <image_file> <username>@<NMC_ip_address>:\<image_file>”
  2. Use ssh to log into NMC, issue “upsfwupdate -install -file A:\<image_file>” command to start upgrading UPS firmware.

Example

  • NMC IP address is 10.191.15.107
  • Username is apc.
  • Image file: SRTL1034UPS_06-7.enc (could be different depending on UPS ID and FW you are uploading)
  • OS: Windows 10

C:\fw_image>dir

Volume in drive C is Windows

Volume Serial Number is C0FF-E65A

Directory of C:\fw_image

09/19/2024  05:06 PM    <DIR>          .

09/19/2024  05:06 PM    <DIR>          ..

08/14/2024  08:56 AM         1,601,152 SRTL1034UPS_06-7.enc  <- firmware image file on local PC.

1 File(s)      1,601,152 bytes

2 Dir(s)  240,162,951,168 bytes free

C:\fw_image>scp SRTL1034UPS_06-7.enc apc@10.191.15.107:\SRTL1034UPS_06-7.enc <- transfer file to NMC.

apc@10.191.15.107's password:

SRTL1034UPS_06-7.enc                                                   100% 1556KB 161.6KB/s   00:09

C:\fw_image>ssh apc@10.191.15.107 <- ssh into NMC.

apc@10.191.15.107's password:

Schneider Electric                      Network Management Card AOS    v2.5.0.8

(c) Copyright 2023 All Rights Reserved  Smart-UPS APP                  v2.5.0.6

-------------------------------------------------------------------------------

Name      : apc753330                                 Date : 09/19/2024

Contact   : Unknown                                   Time : 17:08:13

Location  : Unknown                                   User : Super User

Up Time   : 1 Day 6 Hours 44 Minutes                  Stat : P+ N4+ N6+ A+

-------------------------------------------------------------------------------

IPv4               : Enabled            IPv6               : Enabled

Ping Response      : Enabled

-------------------------------------------------------------------------------

HTTP               : Disabled           HTTPS              : Enabled

FTP                : Enabled            Telnet             : Disabled

SSH/SCP            : Enabled            SNMPv1             : Disabled

SNMPv3             : Disabled           Modbus TCP         : Disabled

BACnet/IP          : Disabled

-------------------------------------------------------------------------------

Super User         : Enabled            RADIUS             : Disabled

Administrator      : Disabled           Device User        : Disabled

Read-Only User     : Disabled           Network-Only User  : Disabled

Type ? for command listing

Use tcpip command for IP address(-i), subnet(-s), and gateway(-g)

apc>dir             <- check the file is uploaded to root folder.

E000: Success

1024 May 12  2023  apc_hw21_aos_2.5.0.8.bin

6795900 May 12  2023  apc_hw21_su_2.5.0.6.bin

45000 Sep 19 17:08  config.ini

0 Jul 22  2023  db/

0 Jul 22  2023  ssl/

0 Jul 22  2023  ssh/

0 Jul 22  2023  logs/

0 Jul 22  2023  sec/

0 Jul 22  2023  fwl/

0 Jul 22  2023  email/

0 Jul 22  2023  eapol/

0 Jul 22  2023  certs/

0 Jul 22  2023  tmp/

0 Jul 22  2023  upsfw/

1601152 Sep 19 17:07  SRTL1034UPS_06-7.enc                <- Firmware has been uploaded to root folder.

apc>upsfwupdate                                                <- Print the help of upsfwupdate command.

E102: Parameter Error

Usage: upsfwupdate  -- Initiate UPS Firmware Update

upsfwupdate <-install <-file filepath | -ver versionspec> [-progress bar] |

-list                           (list available FW versions)

-status [-progress bar] |

-lastresult |

-info <-file filepath | -ver versionspec>>

-- Examples:

-- Get information about version 1.8:

-- apc> upsfwupdate -info -ver "ID18UPS 1.8"

-- Install an update from the USB drive:

-- apc> upsfwupdate -install -file "C:\upsfw\SMT18UPS_09-1.enc"

-- Note: File paths refer to drives attached to the NMC.

apc>upsfwupdate -install -file A:\SRTL1034UPS_06-7.enc         <- Install UPS firmware.

E000: Success

Note

  1. If you encounter “scp: Connection closed” error as shown below when you use scp command to transfer firmware image file to NMC, you need to add “-O” option.

C:\fw_image>scp SRTL1034UPS_06-7.enc apc@10.191.15.107:\SRTL1034UPS_06-7.enc

apc@10.191.15.107's password:

scp: Connection closed

Example of adding “-O” option to force using the original SCP protocol.

C:\fw_image>scp -O SRTL1034UPS_06-7.enc apc@10.191.15.107:\SRTL1034UPS_06-7.enc

apc@10.191.15.107's password:

SRTL1034UPS_06-7.enc                                                                  100% 1556KB 161.6KB/s   00:09

This is the description of “-O” option.

cmd

Other Information

  1. If want to install OpenSSH on Windows system, you can follow the instructions described in this link - Installing and Enabling OpenSSH on Windows.
  2. If you need to download the firmware for SRTL3KRM1UNC, SRTL2K2RM1UNC units, you can download it from this link - https://www.se.com/us/en/download/document/SPD_CLII-AXFCNC_EN/.

Schneider Electric Việt Nam

Phần đính kèm
Using SCP to Upgrade UPS FW.pdf [172.49 KB]