Hôm nay chúng tôi có thể giúp gì cho bạn?

Why UMAC version is V2.0 in license Manager even though UMAC V3.4.3 is activated

Even though the version of UMAC is v3.4.3, the license is the same since v2.0. This will not affect the use of the software and customer doesn't have to worry about that.

License

UMA