Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Why does my APC Surge Arrest or UPS show a Site or Building Wiring Fault when plugged into a Schneider OffGrid Portable Power Station?

Issue:

Why does my APC Surge Arrest or UPS show a Site or Building Wiring Fault when plugged into a Schneider OffGrid Portable Power Station?

Product Line:

Schneider OffGrid Portable Power Station, Back-UPS, Back-UPS Pro, Smart-UPS (120V), Smart-UPS Ultra (120V)

Environment:

All serial numbers

Resolution:

A Site or Building Wiring Fault will show when an APC Surge Arrest or UPS is plugged into a Schneider OffGrid PPS (Portable Power Stations) as the PPS does not have a proper ground. A Surge Arrest or a UPS requires a proper Ground as it's basic requirement to properly protect the loads. It is not recommended to plug in a Surge Arrest or UPS to the PPS and loads should be directly plugged-in to the PPS.

For more information about the Site or Building Wiring Fault, please visit the FAQ below.

Video: What does the Site Wiring Fault Indicator LED on my APC UPS or Surge Arrestor represent?

Plugging in a surge protector into your PPS:

The noise filtration circuitry in a surge protector can effectively "mask" some of the load from the PPS, causing the PPS to report a lower percentage of attached load than there actually is. This can cause a user to inadvertently overload their PPS. Surge protectors utilize MOVs (Metal Oxide varistors) in their circuitry. Nonconforming MOVs in a surge protector connected to a PPS may cause the PPS to report an overload. In addition, a PPS is typically not plugged in to utility power when used. So there is no risk of having a surge to be passed to the loads.

Plugging a UPS into your PPS:

A UPS functions similarly to a PPS. However, in order for your UPS to get the best power available, a UPS should always be directly plugged into the wall receptacle. A UPS' main function it to detect, monitor, clean utility power, and to give a user ample amount of time, when there are power issues, to save anything they are doing when using a computer. While a PPS, is designed for portability and provide power while offsite.

Should there would be any further concerns, please contact us at https://www.apc.com/us/en/support/