Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Smart UPS Modular Ultra has inaccurate data on the Display and NMC Web Interface

Issue:

The UPS shows data on the display/NMC web interface that is not accurate to what the actual data should be.  There may also be a random alarm code associated with these data issues.

Product Line:

Smart UPS Modular Ultra


Environment:

All models, all serial numbers


Resolution:

The UPS firmware has been improved to eliminate false detection of these alarms and inaccurate data.

Please upgrade the UPS to at least firmware 17.0, then clear all alarms if needed.

In order to upgrade the UPS properly, please use the following FAQ - https://www.apc.com/us/en/faqs/FAQ000261838/