Hôm nay chúng tôi có thể giúp gì cho bạn?

IDP10-T SET GDB

  1. Press the NEXT button 2 times and CONFIG will be displayed.
  2. Press ENTER and POLLADR will be displayed
  3. Press NEXT 15 times and SET GDB will be displayed
  4. Press ENTER and ClearDB will be displayed
  5. Press ENTER and transmitter will reset to default parameters.
  6. Complete