Hôm nay chúng tôi có thể giúp gì cho bạn?

An XD2GA is installed on a console plate, the customer cannot remove the rod from the manipulator to install it, how to do ?

The solution is to put out the gasket, not so easy, with the small screw driver, then it will be possible to put out the black screw and then dismantle the product.