Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How to change decimal resolution (2 digits, 3 digits, 4 digits ect) in PME Estidama gadget Period over Period graph.

Environment:

Power Monitoring Expert 2022, 2023, 2024

----------------------------------------------------------------------

Product Line:

Estidama gadget.

----------------------------------------------------------------------

Description of the issue:

If the customer wants to change the decimal resolution of the displayed value in this gadget, then how can they do that.

----------------------------------------------------------------------

Workaround:

It can be done by editing the "EstidamaPeriodOverPeriod.JS" JavaScript file from the folder mentioned in step 1.

Step 1:

Please edit EstidamaPeriodOverPeriod.JS file from the below location and change the precision value accordingly based on the requirement.

“C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\Applications\Dashboards\Content\Gadgets\EstidamaPeriodOverPeriod”

Please refer to the below snapshot to modify the precision value.

Image 1

eg:  Customer can change the precision from 3 to 2 if the customer wants to show 2 decimal values in the report.

Step 2:

Please ensure that the program file path may be different in your installation. Help yourself to find the PME installation path, and edit the java script file.

Step 3:

Once modified, just refresh the browser.