Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Disabling TLS 1.3 in Geo SCADA Expert (August 2024 Update and Later)

⚠️*Warning: This article contains information about editing the registry. Improper changes to the registry can permanently damage the operating system.
Always backup the registry before making any changes.*

Starting with the Geo SCADA Expert August 2024 update, a new registry setting was introduced that allows users to disable TLS 1.3 specifically for Geo SCADA, without impacting the system-wide TLS configuration managed by Schannel.

To (temporarily) disable TLS 1.3 on a Geo SCADA server, follow these steps:

  1. Open the Registry Editor (regedit).
  2. Navigate to the following key:
    HKEY_LOCAL_MACHINE\SOFTWARE\Schneider Electric\ClearSCADA\SCXCom
  3. Create a new String Value named:
    EnableTLS13
  4. Set its value to:
    - "False" to disable TLS 1.3
    - "True" to enable TLS 1.3 (default behavior)

Note: This registry key is not created automatically. If it is missing, Geo SCADA will treat it as "True" by default.

Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Tìm hiểu thêm
Sản phẩm: