Hôm nay chúng tôi có thể giúp gì cho bạn?

ETE - FAQ - Logger: What is the harmonised tariff code for EcoStruxure Transformer Sensor?

The import code and description for the sensor is:

8541.51.1290 - Semiconductor based sensors used to detect electrical, physical and chemical indicators

The codes and tariff rate for each country can be found in the list below.

  • New Zealand: 8541510000G Semiconductor-based transducers, tariff rate: 0%
  • Singapore: 85415000 - Other semiconductor devices, tariff rate: 0%
  • Indonesia: 85415000 - Other semiconductor devices, tariff rate: 0%
  • Thailand: 85415100000 - Semiconductor-based transducers, tariff rate: 0%
  • Malaysia: 85415000 - Other semiconductor devices, tariff rate: 0%
  • Hong Kong: 8541500 - Other semiconductor devices, tariff rate: 0%
  • UAE: 85415100 Semiconductor-based transducers, tariff rate: 0%
  • Italy: 8541510000 - Semiconductor-based transducers, tariff rate: 0%
  • France: 8541510000 - Semiconductor-based transducers, tariff rate: 0%
  • Germany: 8541510000 - Semiconductor-based transducers, tariff rate: 0%
  • Spain: 8541510000 - Semiconductor-based transducers, tariff rate: 0%
  • Canada: 8541510000 - Semiconductor-based transducers, tariff rate: 0%
  • Peru: 8541510010 Of apparatus of headings 85.18, 90.25, 93.05, 93.06 and 95.04- rate: 6%; 8541510090- others, rate: 0%
  • Chile: 85415100 - Semiconductor-based transducers, tariff rate: 6%
  • Brazil: 85415010 Other semiconductor devices- Unmounted, or 85415020- mounted; tariff rate for both: 5.4%
  • Columbia: 8541510000 - Semiconductor-based transducers, tariff rate: 0%
  • Costa Rica: 854151000000 - Semiconductor-based transducers, tariff rate: 1%
  • Mexico: 8541500100 - Semiconductor-based transducers, tariff rate: 0%
  • USA: 8541510000 - Semiconductor-based transducers, tariff rate: 0%
  • UK: 8541510000 - Semiconductor-based transducers, tariff rate: 0%