Hôm nay chúng tôi có thể giúp gì cho bạn?

Is it possible to use a ZBRA1-active antenna with the EcoStruxure Panel server?

Yes, ZBRA1 active antenna can be used with the EcoStruxure Panel server. However, ZBRA1 is not compatible with PowerTag field device.