Hôm nay chúng tôi có thể giúp gì cho bạn?

Is a recovery USB available for PSA6 ?

No, recovery USB is not available to be purchased.

The user can create a recovery USB from the Recovery Utility feature provided on the HMIPSA6 Launcher.

Prepare a commercially available USB memory with a size of 32 GB or more, to create a recovery USB and follow the steps below:

  • 1. Disconnect all connected devices from the product.
  • 2. Insert a commercially available USB memory.
  • 3. Open the Launcher on the desktop.
  • 4. Select the Recovery USB icon.
  • 5. Select the USB memory in Select a disk menu.
  • 6. Select Start.
  • 7. In the confirmation screen, select OK.
  • 8. When completed, select OK.