Hôm nay chúng tôi có thể giúp gì cho bạn?

Default Login Credentials for Sage RTU Legacy C3413 Green CPU

Issue:
Unable to log in to the Sage RTU C3413 (Green CPU) due to unknown or forgotten credentials.

Product:
Sage RTU, C3413 – Green CPU variant

Environment:
Device: Sage RTU C3413
CPU Type: Green CPU
Access Method: Web interface or serial console
User Role: Administrator

Cause:
The default login credentials are required for initial access or after a reset. Users may be unaware of the factory-set username and password.

Resolution:
Use the following default credentials to log in:

  • Username: Admin
  • Password: Admin