Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How to resolve "Cannot launch ModbusDrv.exe" error message when trying to connect via USB cable to an M221?

Issue

When trying to connect to an M221 using Machine Expert Basic using a USB cable I get a "Cannot launch ModbusDrv.exe" error message and I'm not able to connect.

Product Line

Machine Expert Basic, M221

Environment

Machine Expert Basic

Cause

There is an issue with the M221 driver

Resolution

To resolve this issue, the driver needs to be reinstalled. Steps to reinstall it:

1/ Go to: "C:\Program Files (x86)\Common Files\Schneider Electric Shared\M221"

By default the driver is installed on this location after EME Basic is installed.

2/ Right-click on the M211_Controller.inf file and select Install.

3/Try connecting to the M221 again.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)