Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Sage RTU DNP3 Secure Authentication version (DNP SA) Compatibility

Issue:

Customer requests confirmation whether the Sage RTU products supports DNP3 Secure Authentication  (DNP SA), along with guidance on upgrade paths and options to meet security requirements.

Product:

SAGE 2400

SAGE 3030M

SAGE  4400

SAGE 14x0

Environment:

  • Multiple substations standardized on Sage RTUs with standard DNP3 (non-SA)
  • Organizations-wide push to adopt more secure DNP3.
  • Installed base includes hardwired I/O connected via expansion cards.

Cause:

  • The Sage RTU’s DNP3 implementation supports only up to a specific Secure Authentication Version.
  • No further firmware developments about DNP SA will be released.
  • Achieving DNP3 SAv5 or higher would require newer hardware.

Resolution:

  • Current Capability: The Sage RTUs supports DNP3 SAv2 only; it does not support SAv5/SAv6.
  • Roadmap / Firmware: There is no indication for a new firmware releases enabling SAv5+ on Sage RTUs.
  • Recommended Path: To attain DNP3 SAv5 or newer, plan to transition to Powerlogic T500 hardware.
  • Gateway Options: If an interim solution is needed, explore secure gateway approaches; however, validation and compatibility with Sage environments should be confirmed case-by-case.

Next Steps:

    1. Engage Marketing/Offer Management for roadmap, timelines, validated gateway options, and migration guidance.
      • Point of contact: T500 Offer Manager for US/Canada/Mexico (for accurate, current information).
    2. Assess I/O Migration: For sites with hardwired I/O expansion cards, ensure the proposed solution includes a migration or retention plan (e.g., compatible I/O modules, remote I/O, or structured cutover strategy).
    3. Plan Phased Upgrade: Prioritize high-risk substations, conduct a pilot with Powerlogic T500, and verify DNP3 SA configuration, interoperability with the SCADA/EMS, and commissioning procedures.
    4. Document Cybersecurity Posture: Update site standards and commissioning checklists to reflect SA keys management, authentication policies, and fallback behavior.