Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
In Control Expert I am unable to modify custom library/librairies because of a locked message

Product

Control Expert, any version

Issue

User can't create or remove families from their Custom Lib. The error message is "Library database is locked by another process"

running as admin solved the issue, but customer would like to know which folders the software needs admin access to in order to check with his IT group to modify permissions for his windows user login.

Resolution

Try running the Control Expert software as admin with "run as admin" option on the icon and see if that solves the problem.

If it does, but you can't always run the software with admin privileges, you'll need to modify the privileges or your Windows user on this folder (it needs to have read/write privileges on it)

C:\ProgramData\Schneider Electric\Control Expert XX.X (where XX.X is the software version)

library location

Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Tìm hiểu thêm
Sản phẩm: