Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Which SNMP OID can I use to display the APC Network Management Card information?

Issue:
Looking for the SNMP OID to display the Network Management Card information.

Product:
APC Network Management Cards and Network Managed Devices - All Serial Numbers


Answer:

The OID 1.3.6.1.2.1.1.1.0 corresponds to the sysDescr object in SNMP (Simple Network Management Protocol). This object provides the following textual description of a network device’s system:

  • Details about its hardware - (Model / SKU and Serial Number)
  • Firmware - (APC Operating System, Application Module, and Boot Monitor if Applicable to the model)

Below is an example of what data it will give once polled in an SNMP browser :

The following image shows a screen shot from an SNMP browser using the object name sysDescr OID

Please contact our Technical Support Agents at 1-800-800-4272 or chat with us at APC by Schneider Electric for any clarifications or questions.