Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What is our Salt Spray rating on a QED-2 Switchboard?

Subject:

Verification of QED2 Switchboard Paint Finish Standards
Issue:

Paint Standard – Humidity and Corrosion Resistance Testing
Product Line:

QED2 Switchboard
Environment:

Replacement Projects / Product Evaluation
Cause:

Product Design and Material Specifications

Resolution:
• Please refer to the attached PDF document, which includes the technical cut sheet for the paint used in QED2 switchboards.
• The document outlines the results of the 1,000-hour salt spray test, demonstrating compliance with corrosion resistance standards.
• This information can be used to verify finish durability in humid or corrosive environments.

Schneider Electric Việt Nam

Phần đính kèm
Paint Std 2018 (3).pdf [183.58 KB]