Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What is the part number for the Harmony P6 power connector?

Issue

What is the part number to order a replacement power connector for the Harmony P6 family?

Product Line

Advanced, Standard and Basic Modular Boxes, Harmony FP6 Modular Displays

Environment

Physical Human Machine Interface power connector

Resolution

The part number for the DC Power connector is HMIZCCNDC1 (5 pcs/set).

The part number for the AC Power connector is HMIZCCNAC1 (5 pcs/set).

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)