Hôm nay chúng tôi có thể giúp gì cho bạn?

Is the wireless switch set pre-paired, or does the customer need to pair it manually?

The XB5RFB01, XB4RFB01 and XB5RMB03 are packs with non-programmable receivers.

That means these packs come with button already paired with receiver in factory and it is not possible to change, remove or add any other button.