Hôm nay chúng tôi có thể giúp gì cho bạn?

Compact DEP217/218 to X80 DAI1602/1604 quick wiring - 990XSM00201

Issue

Migrating an ASBDEP217/218 to a BMXDAI1602/1604 and need to confirm the 990XSM00201 quick wiring cable pinout.

Product line

Modicon X80, M340, M580

Resolution

Below is an image of the pinout.

wiring pinout