Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How to restart Easy UPS 3S after Emergency Power Off (EPO) activation?

Issue

How to restart Easy UPS 3S after Emergency Power Off (EPO) activation?

Product Line

Easy UPS 3S

Enviroment

  • All Easy UPS 3S models
  • All firmware versions
  • EPO is configured in default mode (turns off rectifier, inverter, charger, and static bypass immediately)

Cause

The EPO button was pressed, shutting down power delivery for safety.

Resolution

Follow these steps to restore normal operation:

  1. Release the EPO button.
  2. Clear the alarm:
    • Go to Function Settings (key icon) → Function → Clear Alarm → Confirm.
  3. Turn on the battery relay:
    • Go to Battery Status Information (battery icon) → Battery Relay → On → Confirm.
  4. Wait 3–5 minutes for the inverter to turn on and the UPS to resume normal mode.

Important Notes:

  • Ensure the emergency condition is resolved before restarting.